BRAKE#.STATE
Description
Reads whether the brake is released or applied.
| Value | Description |
|---|---|
| 0 | Brake applied |
| 1 | Brake released |
Examples
Context
For more information see Brake.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3105 |
1 |
3105 (0xc21) |
BRAKE1.STATE |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
BRAKE1.STATE |
3105 |
Unsigned8 |
Read Only |
- |